CAP#.ARM

Description

Arms or disarms the capture channel.

The capture channel needs to be armed to start the process of monitoring the trigger input and sampling the source on the selected edge. Setting CAP#.ARM to zero will stop the capture process.

After each capture event, CAP#.ARM is reset to 0 and must be armed again by setting CAP#.ARM to 1, before another value can be captured. If CAP#.REARM is 1 or 2 then CAP#.ARM stays at 1 and keeps capturing new values until CAP#.ARM is set to zero.

Examples

Usage

0: Disabled (default)

1: Armed

Code

-->CAP1.ARM 1
-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read/Write
Units N/A
Range

0 to 1

Default Value 0
Data Type Integer
See Also CAP#.REARM
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

CAP1.ARM

31000

7918

Unsigned8

Read/Write

-

CAP2.ARM

31001

7919

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.ARM

31000

Unsigned8

Read/Write

-

CAP2.ARM

31001

Unsigned8

Read/Write

-